NVM Content:	                        NVM Region Name: 	           Description
Extended Address:	                ZCD_NV_EXTADDR:	                   IEEE Identification Address (specific to each device)
Personal Area Network (PAN) ID:	        ZCD_NV_PANID:	                   4 byte ID used to represent the PAN
Extended PAN ID (EPID):                 ZCD_NV_EXTENDED_PAN_ID:	           By default the 64-bit EPID is set to the IEEE Address of the device.  This value could be used during network joining  instead of the 16 bit short address
On a Network Flag:	                ZCD_NV_BDBNODEISONANETWORK:	   Boolean used to represent if the device is part of a network (1= On NWK, 0= Not on NWK)
Group Table:               	        ZCD_NV_GROUP_TABLE:	           Indicates the groups that have been formed between sets of end points in the network
Network Information Base (NIB):	        ZCD_NV_NIB:	                   Contains the attributes required to manage the network layer of the device
Active Key Information:	                ZCD_NV_NWK_ACTIVE_KEY_INFO:	   The network key actively in use
Alternate Key Information:	        ZCD_NV_NWK_ALTERN_KEY_INFO:	   Latest alternate key proposed by the coordinator. 
Network Security Table:	                ZCD_NV_EX_NWK_SEC_MATERIAL_TABLE:  Stores the frame counter and the extended PAN ID of the ZC device 
Trust Center Link Key (TCLK) Table:	ZCD_NV_EX_TCLK_TABLE:	           Table which includes the TX/RX frame counters, extended address, key attributes/type, and the seed shift index of the corresponding devices added to the network
TCLK Install Codes Table: 	        ZCD_NV_EX_TCLK_IC_TABLE:	   Table which includes the key and address of corresponding devices added to the network through the use of install codes